990-5994B-001

Connect the Power Cables

  1. Connect the PE cable to the PE busbar.

    3:3 UPS System

    3:1 UPS System

  2. Connect the input/bypass cables to the maintenance bypass switch MBB.
  3. Connect the UPS output cables to the system isolation breaker SIB.
  4. Connect the load cables.
  5. Fasten the cables with cable ties to the cable reliefs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?