990-93333-001

Applicable Model List

NOTE: The backfeed kit is only applicable for UPSs with one internal switch. The commercial references for the UPSs with one internal switch are listed as follows.
  • Galaxy PX UPS 100 kW scalable to 250 kW 400 V, 1 switch, for external batteries (GPXUPS100K250QBH)

  • Galaxy PX UPS 100 kW scalable to 250 kW 400 V, 1 switch, for external batteries, start-up 5x8 (GPXUPS100K250QBHS)

  • Easy UPS 3-Phase Modular 50 kW scalable to 250 kW 400 V, 1 switch, for external batteries (EMUPS50K250QBH)

  • Easy UPS 3-Phase Modular 50 kW scalable to 250 kW 400 V, 1 switch, for external batteries, start-up 5x8 (EMUPS50K250QBHS)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.