990-5938A-001

Environment

  Operation Storage
Temperature

0 °C to 40 °C ( 32 °F to 104 °F )

-25 °C to 55 °C (-13 °F to 131 °F)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?