990-5938A-001

Prepare the Battery Breaker Box for Cables

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or grommets with the gland plates installed, and do not drill or punch in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Loosen the bolts from either the top or bottom gland plate and remove the gland plate.

    Front Bottom View of the Battery Breaker Box

    Front Top View of the Battery Breaker Box

  2. Drill or punch holes for cables or grommets in the gland plate(s).
  3. Install grommets (if applicable) and refit the gland plate(s).
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.

    Front Bottom View of the Battery Breaker Box

    Front Top View of the Battery Breaker Box

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?