990-5938A-001

Torque Specifications

Bolt size Torque
M6 5 Nm (3.69 lb-ft)
M10 30 Nm (22 lb-ft)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?