990-5454C-001

Install Batteries in the Empty Battery Cabinet

WARNING
unexpected equipment handling
The battery cabinet must not be moved after the batteries have been installed.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Place the batteries on the shelves in the empty battery cabinet and interconnect the batteries.
    NOTE: Do not cover the holes in the corners of the shelves that are intended for cable routing between the shelves.

    Front View of the Empty Battery Cabinet

  2. Note down the battery configuration on the label in the empty battery cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?