Position the Empty Battery Cabinet
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Leave the empty battery cabinet covered while making anchoring
holes to prevent dust or other conductive parts in the system.
Failure to follow these instructions will result in death or serious injury.
|
- Only for installation with two empty battery cabinets: Remove the indicated side panels from the battery cabinets on the
adjacent sides.
WARNINGHazard of arc flash- Do not make mechanical changes to the product (including removal of cabinet parts or drilling/cutting of holes) that are not described in the installation manual.
- The side panels of each individual cabinet must be installed in all installation types (including parallel installations with no air gap between the frames or in installations where the right-most cabinet and/or the left-most cabinet is placed against a wall). Two empty battery cabinets bayed together will be considered as one cabinet and must have side panels installed on the left side and the right side.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
- Position the empty battery cabinet(s) in the final installation
area.NOTE: Leave 100 mm free space behind the empty battery cabinet(s) for airflow.
- Anchor the rear anchoring brackets to the floor.
- Only for installation with two empty battery cabinets: Install the top baying brackets between the empty battery cabinets.
- Remove the indicated four covers.
DANGER