Connect the Power Cables
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Perform a total power off of the UPS system before connecting
the battery cables to the battery circuit breaker box.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
For TT and TN systems each stand alone cabinet of the
system must be individually connected to the protective earthing terminal
in the distribution board that supplies the system.
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
hazard of arc flash
Use the provided M10 bolts and nuts to connect the power
cables.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
- Lockout/Tagout the battery circuit breaker.
- Route the PE cables from the UPS through either the top or bottom of the battery circuit breaker box and connect.
- Route the DC cables from the UPS through either the top
or bottom of the battery circuit breaker box and connect (DC+, N,
DC-).
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHReinstall the inner cover in the top of the battery circuit breaker box before continuing with the installation.Failure to follow these instructions will result in death or serious injury. - Route the battery cables from the battery bank through
the bottom of the battery circuit breaker box and connect (Batt+,
N, Batt-).
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH- Reinstall the inner cover in the bottom of the battery circuit breaker box before continuing with the installation.
- Ensure correct polarity.
Failure to follow these instructions will result in death or serious injury. - Attach the cables to the cables reliefs in the left side, the top, and the bottom of the battery circuit breaker box.
WARNING