990-5938B-001

Mount the Battery Circuit Breaker Box to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the battery circuit breaker box to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware for the type of wall to mount the battery circuit breaker box to the wall.
Failure to follow these instructions can result in injury or equipment damage.
  1. Measure and mark the four mounting hole locations on the wall.
  2. Drill holes in each of the four marked locations.
  3. Loosen the three screws and open the inner door.

    Front View of the Battery Circuit Breaker Box

  4. Lift the battery circuit breaker box, position it against the wall and line it up with the four holes. Fasten with four M10 screws.
    NOTE: Four M10 x 30 torx and nuts are supplied for mounting the battery circuit breaker box to a battery rack. If the battery circuit breaker box is mounted to a wall, use suitable mounting equipment.