990-5938B-001

Installation Procedure

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Place the battery circuit breaker box as close to the battery bank as possible to limit the length of unprotected battery cable.
Failure to follow these instructions will result in death or serious injury.
  1. Mount the Battery Circuit Breaker Box to the Wall.
  2. Prepare the Battery Circuit Breaker Box for Cables.
  3. Connect the Signal Cables for Easy UPS 3S.
  4. Connect the Power Cables.
  5. Final Installation Steps.
For moving or decommissioning the maintenance bypass panel after installation has been completed, see Decommission or Move the Battery Circuit Breaker Box to a New Location.