990-91190B-001

Connect the Power Cables

  1. Connect the PE cables to the PE busbar.

    Front View of the Maintenance Bypass Panel

  2. Connect the input cables to the maintenance bypass switch MBB.
  3. Connect the UPS 1 output cables to the unit output switch 1 UOB1.
  4. Connect the UPS 2 output cables to the unit output switch 2 UOB2.
  5. Connect the system output cables to the system output cables landings.
  6. Fasten the cables with cable ties (provided) to the cable reliefs.