990-91190B-001

Electromagnetic Compatibility

NOTICE
Risk of electromagnetic disturbance
This is a product Category C3 according to IEC 62040-2. This is a product for commercial and industrial applications in the second environment - installation restrictions or additional measures may be needed to prevent disturbances. The second environment includes all commercial, light industry, and industrial locations other than residential, commercial, and light industrial premises directly connected without intermediate transformer to a public low-voltage mains supply. The installation and cabling must follow the electromagnetic compatibility rules, e.g.:
  • the segregation of cables,
  • the use of shielded or special cables when relevant,
  • the use of grounded metallic cable tray and supports.
Failure to follow these instructions can result in equipment damage.