Firmware Update
Presentation
Update the Panel Server to the latest version to:
-
Obtain the latest features
-
Keep up to date with security patches
-
Allow the Schneider Electric Customer Care Center to remotely access the Panel Server webpages.
Remote access certificates for each firmware version are valid up to the dates indicated in the table.
Panel Server firmware version Remote access certificate validity date 002.002.000
27 January 2026
002.001.000
24 November 2025
002.000.000
22 May 2025
Use the latest version of EcoStruxure Power Commission to update your product to the latest available version. It is also possible to perform a firmware update using the embedded webpages.
All firmware designed for the Panel Server is signed using the Schneider Electric public key infrastructure to provide integrity and authenticity of the firmware running on the Panel Server.
Availability
This function is available on Panel Server Entry, Universal, and Advanced.
Checking the Firmware Version
-
With EcoStruxure Power Commission software
-
On the Panel Server webpages at
The latest security patch is also available on the EcoStruxure Panel Server webpages. It is the lowest firmware revision that the Panel Server can be downgraded to, without removing currently installed security patches.
Firmware Compatibility
You can find the device firmware baseline for all communicating devices in the switchboard to check compatibility of firmware versions in the Information menu of EcoStruxure Power Commission software.
When selecting the firmware to install, take into consideration the following criteria and select the corresponding firmware:
-
EcoStruxure Panel Server model, Entry, Universal, Universal Wired by Design, or Advanced.
-
The hardware version, 001.000.000 or 002.000.000. To check the hardware version, refer to the specific topic.
Updating the Firmware
To update Panel Server firmware, use one of the following:
-
EcoStruxure Power Commission software
(recommended) -
Panel Server webpages
For more information about updating Panel Server firmware, refer to the respective release notes:
-
DOCA0249•• EcoStruxure Panel Server Entry - Firmware Release Notes
-
DOCA0178•• EcoStruxure Panel Server Universal - Firmware Release Notes
-
DOCA0248•• EcoStruxure Panel Server Advanced - Firmware Release Notes