DOCA0249EN-09

Firmware Version 001.006.000

Description

Firmware initial version for EcoStruxure Panel Server Entry.

General Features

The following table presents the availability of general features on Panel Server Entry in firmware version 001.006.000.

Available

Not available

General features

Availability

Functionality

Connection to Edge Control (EcoStruxure Power Monitoring Expert, EcoStruxure Power Operation,EcoStruxure Building Operation, any Building Management System, or third-party monitoring or supervision system)

Wi-Fi

2.4 GHz

5 GHz

IEEE 802.15.4 communication

Up to 20 wireless devices as combination of:

  • PowerTag Energy sensors

  • PowerLogic Tag energy sensors

  • Acti9 Active

  • wireless indication auxiliaries for ComPacT and PowerPacT circuit breakers

  • wireless CO2 sensors

  • wireless temperature and humidity sensors

  • PowerTag A

  • PowerTag Ambient

  • Easergy TH110/CL110 environmental sensors

  • PowerLogic HeatTag sensors

Human Machine Interface (HMI)

FDM128 Ethernet display

PowerTag Link display

Backup restore

Backup and Panel Server configuration restore by using Panel Server webpages and EcoStruxure Power Commission software

Configuration

User management by single user account

User management by multiple users with Role-Based Access Control (RBAC)

Alarms

Publication of alarms related to:

  • Communication issue between a device and Panel Server when available from the end devices

  • The three levels of alarms from HeatTag sensors

Protocols

Modbus TCP/IP server

DHCP client

DHCP server

DPWS server

HTTPS

SFTP client

Data export

Panel Server webpages for publication on SFTP server

Publication on Schneider Electric cloud by using Panel Server webpages

Commissioning and Monitoring Features

The following table presents the availability of commissioning and monitoring features on Panel Server Entry in firmware version 001.006.000.

Available

Not available

Commissioning and monitoring features

Availability

Firmware update

Applied to one Panel Server gateway by using EcoStruxure Power Commission software

Applied to one Panel Server gateway by using Panel Server webpages

Applied to several Panel Server gateways by using EcoStruxure Power Commission software

Applied to several Panel Server gateways by using Panel Server webpages

Backup restore

Backup restore on a Panel Server of the same model by using EcoStruxure Power Commission software

Backup restore on a Panel Server of the same model by using Panel Server webpages

Configuration

Configuration by using EcoStruxure Power Commission software

Ethernet configuration for upstream communication by using Panel Server webpages

Selective pairing of wireless devices by using EcoStruxure Power Commission software

Selective pairing of wireless devices by using Panel Server webpages

Monitoring

Display of data of the supported devices (see commercial references in Supported Devices) by using Panel Server webpages

Diagnostic by using Panel Server webpages

Performance and Limitations

  • Performance and limitations on Panel Server Entry:

    • When SFTP publication is enabled, alarms are displayed in the Panel Server webpages but are not published on SFTP Server.

    • The typical response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 30 ms.

    • The maximum response time to Modbus TCP/IP request for a wireless IEEE 802.15.4 device is 1 s, set up Modbus/TCP client timeout accordingly.

    • Wi-Fi function available through a connection to a Wi-Fi infrastructure only. Access point function not available.

  • Limitations on sampling and publishing for Schneider Electric cloud applications:

    • The number of individual data points that can be sampled is limited to 2,000 and limited to a flow of 500 data points per minute.

    • The number of individual alarms that can be configured for monitoring is limited to 100.

  • Limitations on wireless devices:

    • PowerTag Control:

      • Feedback loop in contactor mode is not supported.

      • Configuration in impulse relay mode is not supported.

      • If a PowerTag Control device is connected to a child gateway:

        • No automatic discovery.

        • No data is published to the parent gateway. To be able to publish at the parent gateway level, a custom model has to be developed for the parent gateway.

        • No control function is available through the Panel Server webpages.

        • Pairing process to be followed:

          1. Pair the PowerTag Control devices if any in the configuration (all the other wireless devices must be unpowered).

          2. Pair the PowerLogic HeatTag sensors if any in the configuration.

          3. Pair PowerLogic PD100 if any in the configuration.

          4. Pair the other wireless devices.

    • PowerTag Display: not supported by Panel Server Entry.

    • Limitations on topology publication to the Schneider Electric cloud: all the devices must be connected at least once to the Panel Server to enable the correct topology to be published to the Schneider Electric cloud.

    • Limitations on custom model for wireless devices connected under a child gateway: if a custom model uses the same name as a predefined model and devices are already associated with the predefined model, follow this procedure to load the custom model:

      1. Decommission any device already associated with the predefined model.

      2. Load the custom model in the Panel Server.

      3. Reboot the Panel Server.

      4. Associate the devices with the newly loaded custom model.

      5. Publish the topology in case of use of the Panel Server with a Schneider Electric cloud application such EcoStruxure Asset Advisor or EcoStruxure Resource Advisor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?