DOCA0249EN-11

Panel Server Entry Gateway

Panel Server Entry (PAS400) is a high performance, all-in-one gateway used to retrieve data from IEEE 802.15.4 devices.

Panel Server Entry is a data concentrator for wireless devices (see detailed list).

Panel Server Entry offers the following features:

  • One 10/100BASE-T Ethernet RJ45 port

  • Upstream Modbus TCP/IP connectivity (edge connection)

  • Upstream Wi-Fi connectivity

  • Wi-Fi access point

  • Downstream IEEE 802.15.4 connectivity

  • Data sampling

  • Compatible with the following commissioning tools of Panel Server and connected devices:

    • EcoStruxure Power Commission software

    • EcoStruxure Panel Server webpages

  • Compatible with the following Schneider Electric cloud applications:

    • EcoStruxure Energy Hub

    • EcoStruxure Asset Advisor

    • EcoStruxure Resource Advisor

Convention

EcoStruxure Panel Server is hereafter referred to as Panel Server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?