New Features
-
Data publication through HTTPS, with public certificate authority.
-
Security improvement for Panel Server claiming from EcoStruxure Energy Hub: Claiming procedure uses device code in addition to serial number of Panel Server. The device code is available with the serial number:
-
By flashing the QR code on the front face of the Panel Server
-
on the Panel Server webpages with Panel Server identification data
-
-
For PowerTag C I/O devices, send a schedule for output control from cloud. Once received and running, the function allows the Panel Server to remotely execute scheduled control orders, even if the connection to cloud is interrupted.
-
Improvement in management of remote configurations sent from a cloud application: For invalid configurations, an error is logged in the auto-diagnostic file and feedback is sent to the cloud application to improve troubleshooting.
-
After publishing a topology to the Schneider Electric cloud and receiving the associated remote configuration, the Panel Server displays the following information at :
-
Last remote configuration status
-
Last successful remote configuration date
-
-
For PowerTag devices, addition of reset of energy counters from Energy widget in Monitoring & Control page, with confirmation popup message.
-
New measurements added for applicable wireless devices:
-
Active power demand
-
Peak active power demand with date and time of occurrence
-
Reset of peak active power demand
-
per device on the device page at
-
for all associated devices at
-
-
-
Demand calculation time interval can be set at
-
Panel Server webpage user experience improvements
-
In the Monitoring & Control page, only measurements relevant to the selected device are displayed in Advanced data tab, to improve readability
-
In the Maintenance page, the Panel Server serial number is displayed when Schneider Electric Customer Care Center is authorized to access the Panel Server remotely.
-
Triangular ‘No data’ icon replaced with standard warning icon.
-
-
Diagnostic logs improved for better debugging experience