DUG_Smart Smoke Alarm Battery_WH-00

Removing the device

Using the Wiser Home app, you can remove the smoke alarm from the Wiser system.
  1. On the Home screen, tap .
  2. Tap Devices > Smoke Alarm > Delete (A).
  3. Tap OK to confirm.
    NOTE:
    • Removing the smoke alarm from the app will reset the device. Once reset, the LED will blink amber, indicating that it is ready to pair.

    • If you still have a problem with the reset, refer to Resetting the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.