DUG_SmartDim MW Rotary_WH-01

Pairing Wireless Switch with Rotary Dimmer

  1. Remove the rocker from the Wireless switch.
  2. Short press the top-right push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  3. Remove the knob and short press the push button 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Rotary Dimmer blinks for a few times. The status LED stops blinking green on the Wireless switch and the Rotary Dimmer. The Rotary Dimmer can now be controlled by the Wireless switch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.