DUG_SmartDim MW Rotary_WH-01

Pairing the device with the Wiser Hub

You can pair your dimmer with the Wiser Hub to access and control the dimmer.
  1. On the Home screen, tap .
  2. Tap Devices > > Lights > Rotary.
    TIP: You can also navigate by tapping Control > > Lights > Rotary.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid.

    • (B): Tap this option if you are unable to find the MAC address and Install code.

  4. Tap Next, remove the knob and short press the push button 3 times.
    The LED blinks amber.

    Wait for a few seconds until the LED turns solid green. You can also see in the app that the device is joined.

    NOTE: If the LED is blinking green and red, see the instructions by tapping the link LED blinking green and red?.
  5. Enter the device name in the Name field and tap Next.
    NOTE: The Next button will be enabled after entering a name in the name field.
  6. Select the desired location of the device and tap Submit (B).
    TIP: If you have not created any rooms, enter the room name in the Name (A) field.
    NOTE: The Submit (B) button will be enabled after selecting a desired location.
    IMPORTANT: The next screen shows the Device Settings screen, where you can configure the device settings during the pairing process or later. If you prefer to configure it later, tap Submit. For more information on device settings, refer to the Configuring the device section.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added dimmer on the Control tab under the All and Room tabs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.