DUG_SmartDim MW Rotary_WH-01

Troubleshooting in Quick Home Connect

Symptom

Possible cause

Solution

LED displays amber on the device.

Pairing not completed and returned to factory reset.

Pair the Wireless switch and the device again.

Refer to

Wireless switch not able to control the device reliably.

The Wireless switch and the device are too far away from each other.

Place the Wireless switch in a position closer to the device.

The Wireless switch lost pairing

Pair the device again.

Refer to

The Wireless switch battery is discharged.

Replace the battery of the Wireless switch

Scenario

Procedure

Control multiple devices with one Wireless switch.

To centralize control with one Wireless switch, first pair it with already connected devices. Then, pair the new device to existing group/network.

2-gang Wireless switch with devices (smartswitch smartrelay puck, smart blinds puck, multiwire puck dimmer, push-button dimmer, rotary dimmer, smart blinds push or smart socket).

Pair either left or right Wireless switch with any of the devices (smartswitch smartrelay puck, smart blinds puck, multiwire puck dimmer, push-button dimmer, rotary dimmer, smart blinds push or smart socket). You can also pair another rocker of the Wireless switch with another device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.