DUG_SmartSensor PIR Wireless_WH-00

Example of an automation

This demonstration shows you how to create an automation that turns ON the light in the entrance room at 50 % brightness when motion is detected and a one-minute delay before turning ON the living room light.
NOTE: It is mandatory to create two automations. First, turn on the dimmer light with 50 % brightness when motion is detected. Second, turn off the dimmer light when the motion is no longer detected. 
The dimmer will not turn off automatically until you create another automation.
  1. On the Home screen, tap .
  2. Tap Automations > to create an automation.
  3. Tap Add conditions > Device status change and find your sensor from the list of devices.
  4. Tap Motion Sensor > Motion detection > Detected > Set (A).
    NOTE: No need to set When condition because dimmer turns on when motion is detected.
  5. To add an action, tap Then > Add an action > Control a device > Dimmer.
  6. Set the brightness to 50 % using the sliding bar and tap Set (B).
    TIP: Adding the brightness level will turn on the light when the automation is triggered. You need not add a task to turn on the Dimmer separately.
  7. Tap Add an action > Wait.
    The Add a Wait screen appears.
  8. Select a one-minute time delay duration to trigger an action and tap Set.
  9. Tap Add an action > Control devices > Light.
  10. Tap to turn ON the light.
  11. You can choose the cover image that represents your automation by tapping (C).
  12. Enter the name of the automation (D) and tap Save (E).

Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?