DUG_SmartSensor PIR Wireless_WH-00

Defining Lux setting

Using the Wiser app, you can define the threshold value for lux ranges (such as very dark, dark, bright, very bright) of the environment. This will prevent the false alarm caused by changes in the light intensity.
  1. On the Home screen, tap .
  2. Tap Devices > Motion Sensor > Lux levels (A) to select and define threshold value one of the following option (B):
    • Very dark

    • Dark

    • Bright

    • Very bright

    TIP: Additionally, you can set the sensor lux value by tapping on the Control tab Motion Sensor > Device settings > Lux levels (A).
    NOTE: A lux value represents the present light level in the environment that the sensor measures.

NOTE: In the sensor, the lux value is predefined by default. However, you can change the lux value using the sliding bar; for example, see Very Dark.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?