DUG_SmartSensor PIR Wireless_WH-00

Setting detection delay

Detection delay is the time taken by the sensor to respond after motion is detected.
  1. On the Home screen, tap .
    NOTE: Before applying the new settings, please wake up the sensor (press the function key or simulate the motion).
  2. Tap Devices > Motion Sensor > Detection delay (A) to select one of the following option (B):
    • 15s

    • 30s

    • 45s

    • 60s

    TIP: Additionally, you can set the sensor detection delay time by tapping on the Control tab Motion Sensor > Device settings > Detection delay (A).
    NOTE: Changing the detection delay time from long to short duration shortens battery life.
  3. Tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?