DUG_ELKO - SmartSocket Single 16 A_WH-00

Resetting the device

You can reset the device to factory default manually.
  1. Short-press the push button three times (<0.5 s) and then long-press the push button once (>10 s). The LED blinks red after 10 s, and then release the push button.
    Upon successful reset, the LED stops blinking. Then, the device restarts and blinks green for a few seconds.
NOTE: After reset, the LED turns amber, indicating that the socket is ready for pairing.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.