DUG_ELKO - SmartSocket Single 16 A_WH-00

Resetting the device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:

  • Integrating into ELKO System

    • If you wish to integrate the devices into Wiser Home System, reset all the devices in Quick Home Connect and refer to pairing the device with Wiser Hub.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.