DUG_ELKO - SmartSocket Single 16 A_WH-00

Setting up a schedule

Using the Wiser Home app, you can create or assign a schedule to the Socket outlet.

  1. On the Home screen, tap .

  2. Go to Schedule tab, tap .

  3. Enter the Schedule name and select Appliances from the TYPE menu.
  4. Select the Smart Socket Outlet from the APPLIES TO menu and tap Create.

    The next screen shows by default an Event for the week that can be modified.

  5. Tap to add an event such as STATE (on/off) and WHEN (sunrise/sunset or specific time range).

  6. Tap Set to save the schedule.

    TIP:
    • You can add multiple schedules based on your requirement. Select days, tap , set on/off state and time.

    • You can copy the existing schedule to another schedule or to the days of your choice. Tap .

      • Tap Schedule and select an existing schedule and tap Copy.

      • Tap Day and select the days you want to assign and tap Copy.

    • On the top-right screen, tap and select Follow Schedule toggle switch to turn On/Off the schedule.

    • When the schedule begins, you can see the until time in the following screens:

      • Device Control Screen.

      • Control tab under the device name.

      • Favourite devices section on the home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.