DUG_ELKO - Wiser Underfloor Heating Connection Strip_WH-00

Resetting the device

You can reset the Underfloor Heating to the factory default.
To reset the Underfloor Heating:
  1. Press and hold the Setup button for more than 15 seconds.
    After 15 seconds, the LED flashes red.
  2. When the LED stops flashing red, release the setup button.
    The LED stops flashing upon successful reset of the Underfloor Heating.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.