DUG_ELKO - Wiser Underfloor Heating Connection Strip_WH-00

Emergency Heating

You can do emergency heating manually by pressing the channel button if the Hub is not working or when the Wiser Home app is not responding.
Follow the steps below to do an emergency heating.
  1. Press and hold the Channel Button for >2 seconds.
  2. Press Channel Button again to select further channels.
    The selected channel LED will start flashing.
  3. When the required channel LED is flashing, press and hold for >2 seconds. This LED will be solid green and the next channel LED will flash. You can select and channel combination, e.g., Channels 1, 3 and 5.
  4. Pressing on channel 6 activates the selected channels. The relevant LEDs will flash green and the actuators open to allow water flow.
    After 4 hours an emergency heating stops. The emergency heating can also be stopped by pressing channel button. If multiple Wiser UFH Connection Strips are being used this test can be carried out on all connection strips.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.