Showing 161 - 170 of 272 results

Page 17 of 28
  • LED indications

    ELKO - SmartSensor Climate Wireless – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing User Action LED Indication Status Press the function key 3 times LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off. Resetting User Action LED
  • LED Indications

    ELKO - SmartSensor Leakage Wireless – Wiser Home Device user guide

    LED Indications LED Indications LED Indications Pairing User Action LED Indication Status Press the function key 3 times LED blinks amber , once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off. Resetting User Action LED
  • eSetup App

    Elko Wiser Home – System User Guide (Norway)

    for Electricians App you can, Commissioning of Wiser products with step by step guidance See the complete installation in DEMO Mode (no need of actual devices) Define the system and settings of the devices Verify and test the installation Get connected to Bluetooth or Wifi to the product directly
  • About the device

    ELKO - Wiser Room Thermostat – Wiser Home Device user guide

    information such as (room temperature, relative humidity, battery level, boost status, heating symbol, and signal status). On the Room Thermostat screen, icon changes and appears when the room is in Comfort Mode and when the room is in ECO Mode. For more information, refer to the System User Guide
  • Technical data

    ELKO - Motion Sensor Outdoor, 360 – Wiser Home Device user guide

    °C to 45 °C 10 A 300 W 15 45 °C to 50 °C 8 A 300 W 15 50 °C to 55 °C 6 A 300 W 15 Relative humidity 0 % to 95 %, non condensing Lux setting 1 lx to 2000 lx, Day mode Night mode Sensitivity setting 1 – 6 (50 % - 100 %) Dimensions Ø 82 mm x 107 mm Ø 82 mm x 131 mm with corner bracket Compliance Communication protocol Zigbee ® 3.0 (certified)
  • Creating an automation

    ELKO - Smart Smoke Alarm Battery – Wiser Home Device user guide

    one condition is met. To add condition, tap Add conditions > Device status change > Smoke Alarm and select any of the following (C): Smoke Alarm - When the device detects smoke. Remote Alarm - When the device is triggered by an interconnected device. Test Alarm - When the device is in test mode
  • Configuring the device

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    the device. B Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. C Dimming mode: You can improve the dimming quality in the app if you have problems with light flickering
  • LED indications

    ELKO - SmartSocket Double 16 A – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the push button 3 times LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off. Resetting
  • Adjusting the brightness on the puck

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    with Multiwire puck. Press and hold the left mechanical push button for 15 s. The puck LED blinks green and then the connected load blinks till the settings mode is confirmed. Refer to the following sections for minimum and maximum brightness settings. Some lamps have a starting point. When you turn
  • Setting the room temperature using the app

    ELKO - Wiser Room Thermostat – Wiser Home Device user guide

    time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point. Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system
Page 17 of 28