DUG_ELKO - Wiser Room Thermostat_WH-00

Setting the room temperature using the app

Using the Wiser Home app, you can adjust the room temperature.
On the device control screen, drag the sliding bar up/down to adjust the room temperature.

IMPORTANT:
  • When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point.

  • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

TIP: You can also adjust the room temperature:
  • By tapping or on the Control tab, in the Heating section of the concerned room to adjust its temperature.

  • When you add it to your Favourites. To know more about Favourites, refer to the Managing Favourites topic in the respective System User Guide.

NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.