DUG_ELKO - Wiser Room Thermostat_WH-00

About the device

The Wiser Room Thermostat (hereinafter referred to as Room Thermostat) is a wireless, battery-powered, colorful touch-button display where the end-user can increase, decrease, boost, and set the room temperature.

The Room Thermostat display shows information such as (room temperature, relative humidity, battery level, boost status, heating symbol, and signal status).

NOTE: On the Room Thermostat screen, icon changes and appears when the room is in Comfort Mode and when the room is in ECO Mode. For more information, refer to the System User Guide.

Advantage of using the Room Thermostat:

  • Easy to control all heating appliances in the room from one place.

  • Control locally or remotely using the wiser app

Features of the Room Thermostat:

  • Works with Amazon Alexa & the Google Assistant

  • Boost, and set the room temperature

  • Configure several time schedules for heating

  • To check humidity of the room

  • Device user interface lock

Diagram of operating elements

  1. Reduce temperature

  2. Increase temperature

  3. Boost

  4. LED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.