DUG_SmartDim LED Puck Multiwire_WH-01

Adjusting the brightness on the puck

You can set the minimum/maximum brightness of the puck.
IMPORTANT: Set the minimum/maximum brightness settings of the puck only after pairing it with Wireless switch. Refer Pairing Wireless switch with Multiwire puck.

Press and hold the left mechanical push button for 15 s.

The puck LED blinks green and then the connected load blinks till the settings mode is confirmed.

Refer to the following sections for minimum and maximum brightness settings.

NOTE: Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then goes back to the lower brightness automatically. This is the behaviour of the lamp and the puck can't change it.

Adjusting minimum brightness:

  1. When in brightness settings mode, short press the left mechanical push button 2 times.

    The light reaches the minimum brightness level.

  2. Long press the left mechanical push button to set the minimum brightness of your choice.

    TIP: If you release the push button and then long press it again, it will adjust the brightness in the opposite direction from the previous dimming action (either darker or brighter, based on the prior dimming direction).

  3. Wait for the time out for 30 s or short press the left mechanical push button 2 times to confirm the settings.

    The light blinks for few times indicating that the setting is saved.

Adjusting maximum brightness:

  1. When in brightness setting mode, short press the left mechanical push button 4 times.

    The light reaches current maximum brightness level.

  2. Long press the left mechanical push button, to set the maximum brightness of your choice.

    TIP: If you release the push button and then long press it again, it will adjust the brightness in the opposite direction from the previous dimming action (either darker or brighter, based on the prior dimming direction).

  3. Wait for the time out for 30 s or short press the left mechanical push button 2 times to confirm the settings.

    The light blinks for few times indicating that the setting is saved.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.