Showing 251 - 260 of 272 results

Page 26 of 28
  • Setting Tariff

    Elko Wiser Home – System User Guide (Norway)

    rate to no contract, please change charging mode from Wiser Home AI to Charge Now or Manual or Customized Schedule. Feed in tariff: Feed in tariff will be shown only if you have set the PowerTag for Solar or Solar and Battery which feed electricity to the Grid.The electricity generated from solar or
  • Creating an Account

    Elko Wiser Home – System User Guide (Norway)

    accept. Personalize your consents and tap Continue. Enter your home address and tap Continue. The home address is required so that functions dependent on the location (e.g. to predict the outdoor temperature for Eco-Mode) work properly. Tap to start adding devices to your system. Refer to Adding a Device.
  • Oppretting av konto

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

    dine samtykker og trykk på Fortsett. Skriv inn hjemmeadressen din og trykk på Fortsett. Hjemmeadressen er nødvendig slik at funksjoner som er avhengige av posisjon (f.eks. for å forutsi utetemperaturen for Eco-Mode) skal fungere riktig. Trykk på for å begynne å legge til enheter til systemet. Se Legg til en enhet.
  • Assigning a light group to the Wireless switch

    ELKO - SmartSwitch Push Wireless Plus – Wiser Home Device User Guide

    tap Save. If the device is in sleep mode, press the top-right push button on the Wireless switch 3 times to wake up the device. Then tap Confirm in the app to apply the settings. For more information, refer to Wake up the device. Each group can include up to 60 devices. You can create a maximum of 20
  • Google Home

    Elko Wiser Home – System User Guide (Norway)

    will last until the next event in the Wiser Plug schedule. If the Wiser Plug is running in Manual Mode, everything you tell Google Home to do will remain in place until the next command either from Google Home or from the Wiser Home App. Common Wiser commands for Google Home Listed below are common
  • ELKO - Motion Sensor Outdoor, 360

    screwdriver. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Override modes Override modes This mode temporarily overrides the automatic operation of the motion sensor. For example, it allows you to trigger the load for a set period, even if no motion is
  • Amazon Alexa

    Elko Wiser Home – System User Guide (Norway)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • About the Document

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    -based shutter control, and setting up schedules, moments, and automations. Users can calibrate shutter movement, define device types, and utilize Seasonal Comfort Mode for energy-efficient temperature regulation. The guide also covers managing device settings, updating sensor orientations, and
  • Technical data

    ELKO - Schneider Charge – Wiser Home Device User Guide

    Technical data Technical data Technical data Schneider Charge General characteristics Range Schneider Charge Product name Schneider Charge Product Type AC charging station Pole description 3 P + N / 1 P + N Mounting mode Wall-mounted Rated supply voltage 400 V AC (+/- 10%) 50/60 Hz 3–ph 230 V AC
  • ELKO - SmartDim LED Puck Multiwire

    70 00 elko.no/contact www.se.com Setting Dimming Mode Setting Dimming Mode Using the Wiser Home app, you can manage the Dimmer modes and settings. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 elko.no/contact www.se.com Setting up the Power On Behaviour
Page 26 of 28