DUG_SmartSwitch Push Wireless_WH-00

Assigning a light group to the Wireless switch

You can create light groups and assign them to the left or right push buttons on a Wireless switch.
  1. On the Control tab, tap All devices or the room tab where the Wireless switch is located.
    The Device Control Screen appears.
  2. Tap any key and select Light Group > Continue.
    • If you already have a group and want to continue configuring it with push buttons, follow from step 8.

    • If not, follow the steps below to create a new group.

    TIP: When you reassign a push button to a new action, moment, or group, the screen displays that the existing configuration will be deleted.
  3. Tap + Create a group.
    The New Group screen appears.
  4. Enter a name of the group (A).
    TIP: Tap (B) and choose a suitable icon for your group.
  5. Tap + Add lights.
  6. On the Select Devices screen, choose the devices you want to add, and then tap Save.
    NOTE: Make sure all devices are online before adding them to a group. Offline devices will not appear in the device list.
  7. On the top-right screen of the New Group, tap Save.
    You can see the newly created group under the Groups section.
  8. Select the group and tap Save.
    NOTE: If the device is in sleep mode, press the top-right push button on the Wireless switch 3 times to wake up the device. Then tap Confirm in the app to apply the settings. For more information, refer to Wake up the device.
    IMPORTANT: Each group can include up to 60 devices. You can create a maximum of 20 groups.
    The next screen displays , indicating that the group is successfully assigned.

    Example: If you have four lights (two switches and two dimmers), you can create a group that includes all of them. After assigning this group to the left two push buttons (top and bottom) on the Wireless switch:

    • Short press the left top/bottom push button to turn on/off the devices.

    • Long press the left top/bottom push button to increase/decrease the brightness of dimmable lights.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.