DOCA0212EN-00

Overview of the Application

  • The application is divided into five steps.

  • Navigation within the steps is possible using the tabs at the top of each page.

  • Other functions that are accessible on each page of the application:

    • Register

    • Log in and log out

    • Save a project in the cloud; this is implemented automatically every 2 minutes, when changing step in the application and manually with an action on the corresponding icon.

    • Download a project on the computer

    • Help

    • Terms and conditions

    • About

    • Notes in free text

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?