DOCA0212EN-00

User Price Lists

By default, the application does not embed any price.

To manage the price lists, go to My profile section available in the Main menu.

  • To get the file to be used as a template for price lists, click Download template.

  • Once the file is ready on your computer, click Upload a price list to add it to your profile.

  • A price list can be renamed, downloaded, removed and set as the default one for your future projects.

    NOTE:
    • Up to 10 price lists can be added.

    • A price list can be applied to a project in the Bill Of Material step of the application.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?