DOCA0212EN-00

Switchboard Information

This page allows you to create panels in the project, to manage the description of each switchboard and to manage the list of switchboards in the project.

  • Compulsory data for each panel: Switchboard name.

  • Optional switchboard data:

    • Type of switchboard: main panel or sub panel.

    • Value of the incoming current in the panel.

    • Short circuit current value at the incoming of the panel.

    • Number of phases at the incoming of the panel.

Click the Design button of a switchboard in the list to access the next screen (Bill of Materials) and open the Catalog page.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?