ESXP2GE013EN-05

With Connected Products, Edge Control Software, and Optional Remote Services

In this architecture, the data is collected from all connected products either directly over Ethernet or via gateways. This data is then recorded and processed by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for on-premise visualization, analysis, and reporting.

As an option, data from EcoStruxure Power Monitoring Expert or Power Operation can be passed on to the EcoStruxure Asset Advisor platform and interpreted by experts as a part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.