ESXP2GE001EN-05

Digital Architecture

The digital architecture of the Electrical Distribution Monitoring and Alarming application involves collecting the input data from the different products, either directly over Ethernet or via gateways (such as EcoStruxure Panel Server). These data are then used by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for on-premises visualization, analysis, and reporting.

The most important data from the electrical distribution can also be monitored with a Building Management System (BMS) such as EcoStruxure Building Operation, thanks to seamless integration with EcoStruxure Power Monitoring Expert or Power Operation.

As an option, EcoStruxure XR Operator Advisor Client can be used to enhance Electrical Distribution Monitoring and Alarming with virtually overlaid data on top of equipment and devices.

Data from EcoStruxure Power Monitoring Expert or Power Operation can be passed on to the EcoStruxure Power Advisor platform and interpreted by experts as a part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?