ESXP2GE001EN-05

Inputs

The Electrical Distribution Monitoring and Alarming application collects data from connected products to provide access to consolidated views of electrical measurements, status information, and individual device details. It also monitors remote control actions.

Electrical measurements and status information can be acquired from a wide range of connected products as well as third-party equipment through open communication protocols. Typical connected products include:

Electrical Measurements

The following electrical measurements are collected from connected products (real-time values, the minimum, maximum, and average values):

  • Current and voltage

  • Power (Active, Reactive, Apparent)

  • Frequency

  • Power factor

  • Energy

  • Harmonic distortion

  • Voltage and current unbalance

Status Information and Control Actions

From intelligent electrical devices such as circuit breakers, power quality correction equipment, ATSs, and other electrical distribution equipment:

  • Circuit breaker position (open, closed, racked-in, racked-out, etc.)

  • Circuit breaker trip status, protection status

  • UPS status, motor status

  • Other statuses, operating modes or conditions

  • Control actions (operator or automatic)

Other Physical Measurements

Non-electrical measurements, such as environmental conditions (temperature, humidity, etc.), can also be integrated into the system.

User Input: Alarm Recipient Information and Schedule

For alarm/event notification and distribution, recipient delivery schedules need to be configured.

These schedules are configured to send notifications to the appropriate operators, taking into account shift schedules, holidays, and weekends.

Delivery mechanisms include SMS and SMTP (email).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.