ESXP2GE026EN-05

Electrical Architecture

The following diagram details the areas of the architecture where the connected products should be installed in order to implement the Energy Efficiency Compliance application, in accordance with the guidelines in standards such as ISO 50001, 50002, 50006, IEC 60364-8-1, and IEC 61557-12:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?