Application Outcomes
Live Data Display
Measured energy values such as kWh and peak demand (kW) can be visualized in custom graphical diagrams and live data tables in the Edge Control software.
Events and Alarms
Smart alarms can be configured to alert energy managers or operations staff in case of energy-related events which require attention (imminent exceeding of peak demand threshold, etc.).
Trends
Measured energy values, ratios of measured values, or KPIs (kWh/unit of production, etc.) can be trended in the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation).
Dashboards
-
Energy cost comparison
-
Energy consumption ranking
-
Energy heat map
-
Pareto charts
-
Sankey diagram
-
KPI (Key Performance Indicator) dashboards
-
General line graphs, bar charts, and pie charts
Reports
-
Consumption Ranking Reports
-
Energy Comparison Reports
-
Energy Modeling Reports
-
Energy Usage Reports
-
Calendar Trend Reports
-
KPI Engine Reports
-
Load Profile Reports
-
Energy Cost Reports
Notifications*
SMS or email notifications are sent on pre-alarm and alarm conditions described above to enable fast action.
Cloud-based Analytics and Services
As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor provides data quality analytics with recommendations from our Schneider Electric service experts.