MFR3940104

Loop-through connection

The wall-insert has two screwless loop terminals (X) and an Earth () terminal at the top that can be used to extend cables. These terminals are isolated from the rest of the socket and serve as a replacement for loose terminal blocks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?