MFR3940104

Mounting the product

Wall box adjustment: If applicable, adjust the threaded-screw ring in the wall box such that the outer edge of the threaded-screw ring aligns with the surface of the wall.

NOTE: This step is important to avoid possible deformation of the wall-insert frame while mounting it into the wall box.
  1. Mount the wall-insert into the wall box, with a maximum tightening torque of 0.33 Nm for the screws.
    NOTE: Optional fixing mode by claw kit. (WDE002395)
  2. Remove the protection cap that covers the contact pins on the rear side of the product, before mounting it into the wall-insert.
    NOTE: Any damage to the contact pins; for example, bending, breaking, or deformation, will interfere with the functioning of the product.
    NOTICE
    damage to the contact pins
    • Handle the product carefully to avoid any damage to the contact pins.
    • Make sure that the contact pins do not get damaged while mounting the product into the wall-insert.
    Failure to follow these instructions can result in equipment damage.
  3. Mount the product into the wall-insert using screws.
  4. Remove the protective film covering the surface of the product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?