Install the IP42 Kit on a 1600 mm Wide UPS
WARNING |
|---|
|
TIPPING hazard
Shut down the UPS system completely before installing
the kit.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
- Install the IP42 top assembly:
- Remove the existing fan plates. Save the screws for reuse and discard the fan plates. Install the new fan plates with the reused screws.
- Install the two water guard sheets on the UPS with the four provided M8 screws.
- Install the provided rods on the UPS.
- Install the top covers on the UPS with the eight provided M8 screws.
- Install the gutter between the two top covers and fasten with the six provided M5 screws.
- Install the IP42 front assembly:
- Open the front doors of the UPS.
- Remove the cover plates and the air filters from the front doors. Discard the old air filters and save the screws for reuse.
- Install the new air filters with the reused screws and reinstall the cover plates on the front doors.
- Install the IP42 bottom assembly:
- Remove the kick plates. Save all parts for reinstallation.
- Remove the indicated covers. Save all parts for reinstallation.
- Remove all cables from all the cable openings in the bottom of the UPS.
- Remove the three front screws from the bottom plate and save the screws for reuse. Loosen the three rear screws. Pull the bottom air filters out from towards front. Discard the old bottom air filters.
- Install the new bottom air filter with the reused screws.
- Reconnect the cables and reinstall the kick plates.
WARNING