990-91409A-001

Load Derating for UPS with IP42 Kit Installed

NOTICE
Risk of overheating
  • A UPS with IP42 kit may require load derating / overload derating. See table below.
  • Read all instructions in the installation manual before installing or working on the UPS.
Failure to follow these instructions can result in equipment damage.
UPS rating

UPS commercial reference

Maximum continuous load at 30 °C

Maximum continuous load at 35 °C

Maximum continuous load at 40 °C

10 kW

EPWUPS10KU6PT

8kVA/6.8kW

8kVA/6.4kW

6kVA/5.2kW

EPWUPS10KU12PT

8kVA/6.8kW

8kVA/6.4kW

6kVA/5.2kW

EPWUPS10KU6P

8kVA/6.8kW

8kVA/6.4kW

6kVA/5.2kW

EPWUPS10KH6P

8kVA/6.8kW

8kVA/6.4kW

6kVA/5.2kW

20 kW

EPWUPS20KU6PT

17kVA/13.6kW

16kVA/12.8kW

13kVA/10.4kW

EPWUPS20KU12PT

17kVA/13.6kW

16kVA/12.8kW

13kVA/10.4kW

EPWUPS20KU6P

17kVA/13.6kW

16kVA/12.8kW

13kVA/10.4kW

EPWUPS20KH6P

17kVA/13.6kW

16kVA/12.8kW

13kVA/10.4kW

30 kW

EPWUPS30KU6PT

25kVA/20.4kW

24kVA/19.2kW

19kVA/15.6kW

EPWUPS30KU12PT

25kVA/20.4kW

24kVA/19.2kW

19kVA/15.6kW

EPWUPS30KU6P

25kVA/20.4kW

24kVA/19.2kW

19kVA/15.6kW

EPWUPS30KH6P

25kVA/20.4kW

24kVA/19.2kW

19kVA/15.6kW

40 kW

EPWUPS40KU12PT

34kVA/27.2kW

32kVA/25.6kW

26kVA/20.8kW

EPWUPS40KU6P

34kVA/27.2kW

32kVA/25.6kW

26kVA/20.8kW

EPWUPS40KH6P

34kVA/27.2kW

32kVA/25.6kW

26kVA/20.8kW

50 kW

EPWUPS50KU12PT

42kVA/34kW

40kVA/32kW

32kVA/26kW

60 kW

EPWUPS60KU12PT

51kVA/40.8kW

48kVA/38.4kW

39kVA/31.2kW

EPWUPS60KU6P

51kVA/40.8kW

48kVA/38.4kW

39kVA/31.2kW

EPWUPS60KH6P

51kVA/40.8kW

48kVA/38.4kW

39kVA/31.2kW

80 kW

EPWUPS80KU12PT

68kVA/54.4kW

64kVA/51.2kW

52kVA/41.6kW

EPWUPS80KU6P

68kVA/54.4kW

64kVA/51.2kW

52kVA/41.6kW

EPWUPS80KH6P

68kVA/54.4kW

64kVA/51.2kW

52kVA/41.6kW

100 kW

EPWUPS100KU12PT

85kVA/68kW

80kVA/64kW

65kVA/52kW

EPWUPS100KH12P

85kVA/68kW

80kVA/64kW

65kVA/52kW

100 kW

EPWUPS120KU12PT

102kVA/81.6kW

96kVA/76.8kW

78kVA/62.4kW

EPWUPS120KH12P

102kVA/81.6kW

96kVA/76.8kW

78kVA/62.4kW

160 kW

EPWUPS160KH12P

136kVA/108.8kW

128kVA/102.4kW

104kVA/83.2kW

200 kW

EPWUPS200KH12P

170kVA/136kW

160kVA/128kW

130kVA/104kW

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?