990-91735-001

Configure the External Breakers

  1. On the main menu screen, tap Configuration > External breakers.
    1. Tap the buttons to configure which breakers are Present or Not Present in the UPS system.
    2. Tap the button to configure the breaker asNormally closed or Normally open.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?