Troubleshooting
View the Active Alarms
When there is an active alarm in the system, a symbol indicating the alarm level is shown in the top right corner of the screen and the buzzer is active.
- Tap the alarm status symbol to access the active alarms
log. The log shows the latest 100 events with the newest events at
the top of the list.
- Tap the arrow buttons to scroll up and down.
- Tap Severity, Date,Time or UPS #ID to sort the events.
Alarm Messages
| Alarm/ Event | Severity |
Display text |
Description | Corrective action |
|---|---|---|---|---|
| Alarm | Warning | Ambient temperature high | Ambient temperature is high. | Please check the environment. |
| Alarm | Warning | Ambient temperature out of tolerance | Ambient temperature is out of tolerance. | Please check the environment. |
| Alarm | Warning | Batteries are discharging | The load is drawing more power than the UPS can draw from the input, causing the UPS to draw power from the batteries. | |
| Alarm | Warning | Battery breaker BB1 open | Battery disconnect device BB1 is open. | |
| Alarm | Warning | Battery breaker BB2 open | Battery disconnect device BB2 is open. | |
| Alarm | Warning | Battery breaker BB3 open | Battery disconnect device BB3 open. | |
| Alarm | Warning | Battery breaker BB4 open | Battery disconnect device BB4 open. | |
| Alarm | Warning | Battery condition is poor | Battery capacity is lower than 50%. | Batteries should be replaced. |
| Alarm | Warning | Battery condition is weak | Battery capacity is between 50% to 75%. | |
| Alarm | Warning | Battery float charge current exceeds expected value | The battery float charge current exceeds the expected value and has been limited to avoid thermal runaway. | |
| Alarm | Warning | Battery is below minimum acceptable runtime | The battery runtime is below configured minimum acceptable value. | |
| Alarm | Critical | Battery is not working correctly | A battery is not working correctly. | Please contact Schneider Electric. |
| Alarm | Warning | Battery room ventilation inoperable | Input relay indicates that the battery room ventilation is not working correctly. | |
| Alarm | Warning | Bonding between neutral and ground missing | Bonding between neutral and ground is missing. | |
| Alarm | Warning | Breaker MBB closed | Maintenance bypass disconnect device MBB is closed, feeding the load with unprotected power from bypass. | |
| Alarm | Warning | Breaker SIB open | System isolation disconnect device SIB is open, and system cannot feed the load. | |
| Alarm | Warning | Breaker SSIB open | Bypass static switch input disconnect device SSIB is open, making static bypass operation unavailable. | |
| Alarm | Warning | Breaker UIB open | Unit input disconnect device UIB is open, and the UPS is prevented from running in normal operation. | |
| Alarm | Warning | Breaker UOB open | Unit output disconnect device UOB is open, and UPS cannot feed the load. | |
| Alarm | Warning | Bypass backfeed breaker open | Bypass backfeed disconnect device is open. | |
| Alarm | Warning | Bypass frequency out of tolerance | Bypass input frequency is out of tolerance. | Check bypass input frequency and bypass input frequency setting. |
| Alarm | Warning | Bypass phase missing | Bypass input is missing a phase. | Check bypass input. Please contact Schneider Electric. |
| Alarm | Warning | Bypass phase sequence incorrect | The phase rotation on bypass input is incorrect. | Check bypass input. Please contact Schneider Electric. |
| Alarm | Warning | Bypass voltage out of tolerance | Bypass input voltage is out of tolerance and UPS is prevented from going into requested bypass mode. | |
| Alarm | Warning | Charger shutdown due to high battery temperature | The charger has been shut down due to a high battery temperature. | |
| Alarm | Critical | EPO Switch Activated | An emergency power off (EPO) switch is activated. | Deactivate the Emergency Power Off switch. |
| Alarm | Warning | External battery monitoring detected fault | Input relay indicates external battery monitoring has detected a fault. | |
| Alarm | Critical | External energy storage monitoring: Major alarm | Input relay indicates external energy storage monitoring has detected a major alarm. | Please contact Schneider Electric. |
| Alarm | Warning | External energy storage monitoring: Minor alarm | Input relay indicates external energy storage monitoring has detected a minor alarm. | Please contact Schneider Electric. |
| Alarm | Warning | External signal turns charger off: Activated | Input contact for charger off is activated. | |
| Alarm | Warning | Ground fault detected | Input relay indicates that a ground fault has been detected. | Please contact Schneider Electric. |
| Alarm | Critical | High battery discharge current shutdown | The energy storage surveillance has detected a battery discharge current above shutdown limit. | |
| Alarm | Warning | High Battery Temperature Level | The battery temperature is above the alarm setting. | Check the battery temperature. A high temperature may decrease the battery lifetime. |
| Alarm | Critical | High battery temperature shutdown | The energy storage surveillance has detected a battery temperature above shutdown limit. | |
| Alarm | Warning | Input frequency out of tolerance | Mains input frequency is out of tolerance. | Check input frequency and input frequency setting. |
| Alarm | Warning | Input phase missing | Input is missing a phase. | Check input. Please contact Schneider Electric. |
| Alarm | Warning | Input phase sequence incorrect | The phase rotation on input is incorrect. | Check input. Please contact Schneider Electric. |
| Alarm | Warning | Input voltage out of tolerance | Mains input voltage is out of tolerance. | |
| Alarm | Warning | Internal power module redundancy lost | The configured internal power module redundancy is lost because there are not enough power modules available. | |
| Alarm | Warning | Inverter is Off due to a request by the user | The inverter is off due to a request by the user. | |
| Alarm | Warning | Inverter output is not in phase with bypass input | The UPS inverter output is not in phase with the bypass input. | |
| Alarm | Warning | Load on UPS is above warning level | Load on UPS has exceeded the warning level. | |
| Alarm | Warning | Low Battery Temperature Level | The battery temperature is below the Alarm setting. | |
| Alarm | Warning | MBB redundant monitoring not working correctly | The two redundant AUX switches of MBB do not report the same status. | |
| Alarm | Warning | Neutral displacement detected | Neutral displacement has been detected. | |
| Alarm | Warning | Output frequency out of tolerance | Output frequency is out of tolerance. | Check output frequency and output frequency setting. |
| Alarm | Warning | Output voltage out of tolerance | The output voltage is out of tolerance. | |
| Alarm | Warning | Overload on installation | The load exceeds 100% of rated installation capacity. | |
| Alarm | Warning | Overload on UPS due to high ambient temperature | The load exceeds the rated capacity when running with high ambient temperature. | Reduce load on system or ambient temperature. |
| Alarm | Warning | Overload or short circuit on UPS | Reduce load on system or check for output short circuit. | The load exceeds 100% of rated capacity or there is a short circuit on the output. |
| Alarm | Warning | Parallel breaker status inconsistency detected | The status of one or more common parallel disconnect devices is not detected to be the same on all parallel UPS. | Replace parallel cable 1. |
| Alarm | Warning | Parallel communication lost on PBUS cable 1 | PBUS cable 1 may be damaged. | |
| Alarm | Warning | Parallel communication lost on PBUS cable 2 | PBUS cable 2 may be damaged. | |
| Alarm | Warning | Parallel mixed operation mode | One or more parallel UPS units are operating in battery operation, while others are operating in normal operation. | |
| Alarm | Warning | Parallel redundancy lost | The configured parallel redundancy is lost, either because the output load is too high, or because there are not enough parallel UPS units available. | |
| Alarm | Warning | Parallel unit not present | UPS is unable to communicate with parallel UPS %d. The UPS might have been powered down or PBUS cables may be damaged. | |
| Alarm | Warning | PM (X) Power module disabled | The power module has been disabled. | |
| Alarm | Warning | PM (X) Power module inoperable | Power module is inoperable. | |
| Alarm | Critical | PM (X) Power module overheated | Power module temperature exceeds critical level. | |
| Alarm | Critical | PM (X) Power module surveillance detected fault | Power module surveillance has detected a fault. | |
| Alarm | Warning | Static bypass switch fan inoperable | Static bypass switch has one or more inoperable fans. Fan redundancy is lost. | |
| Alarm | Critical | Static bypass switch inoperable | Static bypass switch is inoperable. UPS is prevented from going into static bypass operation. | |
| Alarm | Warning | Synchronization unavailable - system is freerunning | The UPS is unable to synchronize to the bypass input, external source or parallel system. | |
| Alarm | Critical | System locked in bypass operation | The system is locked in bypass operation. | The system has toggled between inverter operation and bypass operation more than 10 times within 1 minute. Please activate on button to transfer back to normal operation. |
| Alarm | Critical | System operation mode - Forced static bypass | The system is in bypass in response to a critical event or an inverter off request. | |
| Alarm | Warning | System operation mode - Maintenance bypass | The system load is supplied through the maintenance bypass disconnect device MBB. | |
| Alarm | Critical | System operation mode - Off | The system output power is turned off. | |
| Alarm | Warning | System operation mode - Requested static bypass | The system is in bypass in response to the UPS front-panel or a user-initiated software command, typically for maintenance. | |
| Alarm | Critical | System operation mode - Static bypass standby | The system is in static bypass standby operation in response to a critical event or an inverter off request. | |
| Alarm | Warning | Temperature of input and/or output transformer is too high | Temperature of input and/or output transformer is too high. | |
| Alarm | Warning | UOB redundant monitoring not working correctly | The two redundant AUX switches of UOB do not report the same status. | |
| Alarm | Warning | UPS locked in static bypass mode: Activated | Input contact for UPS locked in static bypass mode is activated. | |
| Alarm | Warning | UPS operation mode - Battery | On battery power in response to an input power problem or due to a transfer out of eConversion. | |
| Alarm | Critical | UPS operation mode - Forced static bypass | The UPS is in forced static bypass. | |
| Alarm | Warning | UPS operation mode - Maintenance bypass | The UPS load is supplied through the maintenance bypass disconnect device MBB. | |
| Alarm | Critical | UPS operation mode - Off | The output power is turned off. | |
| Alarm | Warning | UPS operation mode - Requested static bypass | The UPS is in bypass in response to the UPS front-panel or a user-initiated software command, typically for maintenance. | |
| Alarm | Warning | UPS operation mode - Static bypass standby | The UPS is ready to enter static bypass but awaits permission from the system. UPS output is off. | |
| Alarm | Critical | UPS surveillance detected fault | UPS surveillance has detected a fault. | Please contact Schneider Electric. |