990-91386-001

Final Installation

  1. Reinstall the four front covers.

    Bottom Cable Entry System with Battery Breaker

    Top Cable Entry without Battery Breaker

  2. Fasten the front anchoring bracket (saved during the unpacking procedure) to the empty battery cabinet.

    Front View of Empty Battery Cabinet

  3. Mount the front anchoring bracket to the floor.
    NOTE: Floor anchoring bolts are not provided.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?