990-9137889A-001

Configure the Battery Solution

DANGER
hazard of electrical shock, explosion, or arc flash
Battery settings must only be configured by qualified personnel knowledgeable of batteries, battery configuration, and the required precautions.
Failure to follow these instructions will result in death or serious injury.
  1. Tap Configuration > Battery.
  2. Select your battery solution type as Standard and select the commercial reference LIBSESMG16UL or LIBSESMG17UL from the drop-down list as per your configuration.
  3. Tap General settings and set up the following parameters:
    NOTE: On each page, tap OK to save your settings and tap the arrow symbol to go to the next page.
    Number of battery cabinets connected to the battery breaker Shows number of battery cabinets connected to the battery disconnect device. Only configurable by Schneider Electric Service.
    Low runtime warning (sec) Set the threshold for remaining runtime in seconds that will activate the low runtime warning.
    Charge capacity (%) Set the maximum charge capacity in percentage of the UPS nominal power rating.
    Temperature monitoring Shows if temperature monitoring is enabled. Only configurable by Schneider Electric Service.
    Temperature sensor # 1/Temperature sensor # 2 Shows presence of temperature sensors. Only configurable by Schneider Electric Service.
    Minimum threshold Set the minimum acceptable battery temperature in Celsius or Fahrenheit. Temperatures below this threshold will activate an alarm.
    Maximum threshold Set the maximum acceptable battery temperature in Celsius or Fahrenheit. Temperatures above this threshold will activate an alarm.
    Charger autoboost mode Shows charger autoboost mode. This function will automatically transfer the charger to boost charger mode after the system has been in battery operation. Only configurable by Schneider Electric Service.
    Cyclic charge mode Shows cyclic charge mode.

    During a cyclic charge, the system cycles between periods of float charging and resting. This function will continuously maintain the battery charge status without stressing the batteries by conducting a permanent float charging.

    Only configurable by Schneider Electric Service.
    Test interval every Set how often the UPS should run a battery test.
    Test day of the week Set on which day of the week the battery test should run.
    Test start time (hh:mm) Set which time of day the battery test should run.
    Manual battery self-test mode Set which battery test type should run: By capacity or By voltage/time. By capacity will discharge the batteries and use about 10% of the total capacity.
    By voltage/time will discharge the batteries to a set time or voltage.
    Time limit (minutes)/Voltage limit (V) If you chose battery test type By voltage/time, set the time limit or set the voltage limit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.